Question
STEVAL-ESC001V1 example code generate failed
- 3 replies
- 461 views
1. Hardware / Software setup
Board: STEVAL-ESC001V1 (MCU: STM32F303CBTx)
Motor: BullRunning BR2804-1700 kV
STM32 Motor-Control SDK: 5.4.8 (C:\…\MC_SDK_5.4.8)
MC Workbench: 5.4.8.21553
STM32CubeMX: 5.4.0, 5.6.1, 6.4.0
STM32Cube F3 FW: 1.11.3
Target tool-chain: STM32CubeIDE 1.15
Drive type: HAL
2. What I have tried
Deleted the generated folder and ran Generation again → same result.
Re-installed/selected CubeMX 5.4.0, 5.6.1, 6.4.0 → all produce identical errors.
Checked MCSDK release notes – unclear which CubeMX revision is officially supported.
3. Questions
How to use the example code to the eval board
4. Extra information
log is attached; let me know if the .ioc or code snippets are needed.
Thanks in advance for any guidance!