Skip to main content
Amrit Singh
Associate
November 6, 2018
Question

STEVAL-ESC001V1 and Motor Control Workbench 5.2 - Image size exceeds the maximum allowed size

When I use the motor control workbench with KEIL uvision 5.25, I get the following error:

linking...

ESC001\ESC001.axf: error: L6047U: The size of this image (33032 bytes) exceeds the maximum allowed for this version of the linker

Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.

"ESC001\ESC001.axf" - 1 Error(s), 0 Warning(s).

Target not created.

I read somewhere that there are compiler options to reduce code size - which were for AC6. Can anyone guide me towards fixing these errors for uVision.

Thanks!

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards