Skip to main content
Visitor II
January 28, 2025
Question

STEVAL-CTM012V1

I have STEVAL-CTM012V1 evaluation board for 250 W. I have followed all the procedure which are mention in the manual where I first load the firmware file stsw-ctm11 in motor control work bench then click on generate code then goes into cubemx then generate code and goes into STM32CubeIDE and project is created. So my question is that the generated project is enough to run motor means we just need to upload the code into the board and it will start motor right?

 

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
March 4, 2025

Hello @Aditya_sp,

For provided example usage, refer to um2963 documentation, "4 Firmware debug " chapter.
You can use X-CUBE-MCSDK-6 tool available here to generate your project.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA