Skip to main content
Associate II
Feb 6, 2024 10:19 AM UTC
Solved

STEVAL-ctm006V1 startup failure.

Hi,

mcsdk: 6.2.1

control board: nucleo-g474re

Bridge: XNUCLEO-IHM09M2

Power Board: STEVAL-CTM009V1

Motor: Motenergy ME1304

 

I prepared motor profile for ME1306 with help of EVSPIN32G4 and used in configuration,described above.

But now I get Startup failure on every start. The shaft does not rotate but trembles only.

Can I get any advice how to debug the issue?

Appreciate in advance.

    This topic has been closed for replies.
    Best answer
    Feb 21, 2024 9:56 AM UTC

    Hey @tasifacij 

    Here are some screenshots that might help you get a better startup procedure.

    please note that speed feedback, startup failure, and over current errors may  arise due to hardware issues.

    Best Regards!1.png2.png

    9 replies

    tasifacijAuthor
    Associate II
    Feb 6, 2024 10:20 AM UTC

    And I can rotate the motor if open loop is enabled.

    Associate III
    Feb 21, 2024 8:51 AM UTC

    Hi @tasifacij , how did you do the Open loop in ctm009v1? can you provide me some insights on it.

    tasifacijAuthor
    Associate II
    Feb 21, 2024 9:30 AM UTC

    MotorWorkbench -> StageConfiguration -> OpenLoop checkbox.

    Then Motor pilot allows to select it in control mode.

    tasifacijAuthor
    Associate II
    Feb 21, 2024 9:31 AM UTC

    My issue was caused by invalid ICS wiring. I read an inversed signal and PI controllers became crazy of that.

    Best answer
    Feb 21, 2024 9:56 AM UTC

    Hey @tasifacij 

    Here are some screenshots that might help you get a better startup procedure.

    please note that speed feedback, startup failure, and over current errors may  arise due to hardware issues.

    Best Regards!1.png2.png

    Associate III
    Feb 22, 2024 5:13 AM UTC

    thank you @unknown will try as you have mentioned hope it works