Skip to main content
B.Michele
Associate III
March 17, 2021
Question

Stepper Motor Drive L6208 With STM32F100RBT6B

Hy, i must Drive the Clock PIN of the L6208 with the Timer_1-CH1 pin41 or Timer2-CH2 pin42,

it's the same for me (micro STM32F100). There is a routine firmware, a library or a C function, with the configuration and control mode of the Timer_1 to generate the constant duty cycle signal about 50% and variable frequency for example from 200 Hz to 4000 Hz to drive the clock pin of the L6208 ??

Thank you very much

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
March 17, 2021

Output Compare set to Toggle mode in TIMx_CCMRx (and enabled in TIMx_CCER) will produce a 50% output with frequency half of the timer's overflow frequency. As TIM1 is an Advanced timer, don't forget to set TIMx_BDTR.MOE. Of course, the given pin has to be set to AF output in GPIO.

You change frequency by changing TIMx_ARR; it's recommended to have ARR preload set (i.e. TIMx_CR1.ARPE=1).

JW

B.Michele
B.MicheleAuthor
Associate III
March 19, 2021

Thank you Waclawek, Yes this is the evolution Timer, the best, i chose this on purpose!.

Now i use this Timer for PWM function fixed frequency, next week i try to modify this function with your suggestion and library manual for frequency ramps

I'll keep you up-to-date!.

Another Hardware Question, I think to Use The STM L6208 or Toshiba TB6600HG Stepper motor Driver. To reduce the power dissipated by the drivers:

I thought of inserting the 8 recirculation diodes (Fast diode) also externally, so as to slightly reduce the dissipation on the internal diodes during the switching phases. This is because I have to make the most of these 2.4 Ampere bipolar Stepper drivers !! that heat a lot and go into thermal protection even with large radiators... The 0,3 RdSon Mosfet is a little poor... clear that the recirculation diodes dissipate little compared to Mosfets... but to gain something... and a little less heating...

Thank's