Skip to main content
erenes
Associate II
May 14, 2016
Question

Start-up Failure using FOC lib

Posted on May 14, 2016 at 03:18

Hello 

I try to use In-Wheel motor. 300W with Hall sensor.

I used workbench and finally succeeded to run Motor Profiler .

And got motor parameters, PID gains.

After this, applied these parameters and tried to run the motor.

But because of this error, it doesn't run.  ''Start-up Failure''.

I referenced some troubleshoot.  and tried several things.

Like decreasing G2 gain in observer.  and increasing variance threshold in Observer+PLL.  But still didn't work. 

I expected higher current like 1A when  starting up. But my current meter

shows just 0.2A.   Current meter just show overall current not just phase current though. 

Now what can I try?    

(Thanks Gigi for your big help)
This topic has been closed for replies.

2 replies

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards