Question
Start a motor with sensor (using hall sensor) under heavy load situation, the motor will produce noise and motor sometimes can't move successful
I use MCSDK 5.3.2 and our board(which is similar IHM08h but we modify the over current from 30A to 60A) with using hall sensor to drive motor(our purpose is to drive E-bike and E-Scooter)
But i find that in heavy load situation,i will hear motor will produce noise and motor sometimes will fail to move.
Is there any way to improve this parts?
thanks