Skip to main content
Associate
Dec 18, 2024 8:06 AM UTC
Question

St motor workbench CubeMx error

Hi everyone,I have problem about ST Motor Control Workbench.I can ' t generate project.I tried so many things(I installed and unistalled different versions , I changed OS language etc.) but I couldn't do it .Please help.stPic.PNG

This topic has been closed for replies.

25 replies

ilker07Author
Associate
Dec 18, 2024 8:28 AM UTC

power board:B-G431B-ESC1 

ilker07Author
Associate
Dec 19, 2024 8:17 AM UTC

Please any help?

ST Employee
Dec 19, 2024 8:38 AM UTC

Hello @ilker07 

 

could you tell us which version of MCSDK and also STM32Cubemx you have already installed on your PC ?

Thanks in advance

 

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 19, 2024 8:57 AM UTC

MCSDK  ==> 5.4.8

STM32Cubemx==> 6.2.0

 

Thanks in advance

ST Employee
Dec 19, 2024 10:20 AM UTC

@ilker07 ,

 

it seems that the STMC Workbench does not detect correctly the latest version of CubeMx installed.

Can we try to uninstall the Cubemx and reinstall it, and try again please (keeping MCSDKalready installed)?

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 19, 2024 10:26 AM UTC

I installed and unsitalled so many cubemx version.Nothing worked.

ST Employee
Dec 19, 2024 10:41 AM UTC

@ilker07 

 

normally the MC Workbench will detect at least the latest CubeMx version you had installed, that why i propose you to uninstall and reinstall it to check this.

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 19, 2024 10:44 AM UTC

you mean STM32Cubemx verison 6.2.0 or Motor Control Workbench?

ST Employee
Dec 19, 2024 10:47 AM UTC

only uninstall (launch uninstall.bat located in your Cubemx folder) and reinstall STM32CubeMx v6.2.0

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 19, 2024 10:53 AM UTC

I did exactly what you said but it didn't work.

ST Employee
Dec 19, 2024 1:26 PM UTC

Hi @ilker07 ,

I need some inputs :

- can you tell me if you are installing CubeMx with your admin account or not?

- can you check if when editing windows "register editor" in the following path Computer\HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Uninstall you have the Key for your installation of Cube Mx ()

 

Regards

 

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 19, 2024 1:31 PM UTC

q1 ==> yes

 

reg.PNG

ST Employee
Dec 19, 2024 2:09 PM UTC

@ilker07 ,

 

your register key status explains that the MC Workbench cannot detect whether a CubeMx version is installed or not.

Can you check also this key in the following path :  Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\STM32CubeMX

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 19, 2024 2:18 PM UTC

there is no folder named STM32CubeMX after  Uninstall.

ST Employee
Dec 19, 2024 3:23 PM UTC

@ilker07 ,

 

ok all this explain your problematic because the detection of CubeMx version through MC WB GUI is based on those windows keys, and the only way to solve it is to again, sorry but we need to do so again, is to

- uninstall and reinstall STM32CubeMx v6.2.0 or you can use also 6.4.0 which is compatible with MCSDK 5.4.8
- do it with admin rights and select whether you want it to be for you only or all users on the machine.

By the way, do you select the path where to install CubeMx or do you let the default path ?

 

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 20, 2024 6:33 AM UTC

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX

ST Employee
Dec 20, 2024 8:53 AM UTC

Hi @ilker07 ,

 

what did you have in the windows register key now ?

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 20, 2024 11:45 AM UTC

Did you mean HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\STM32CubeMX?

ST Employee
Dec 20, 2024 1:45 PM UTC

@ilker07 ,

 

yes please if you can check this key.

 

Regards

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
ilker07Author
Associate
Dec 20, 2024 4:55 PM UTC

There is nothingnamed STM32CUBEMX reg.PNG