Skip to main content
JEsca.1
Associate II
March 24, 2020
Question

ST Motor profiler with NUCLEO-F401

Dear

I am looking to test Nucleo-F401 with Motor driver IHM07-M1 but when stating motor profiler, this nucleo board does not appears in the list of supported board. When reading release not of Motor profiler, F401 should be in the supported board.

Please help

Thanks

This topic has been closed for replies.

3 replies

Cristiana SCARAMEL
ST Employee
March 25, 2020

You are right the Nucleo-F401RE is not available in the Motor profiler.

Anyway if you have the motor datasheet you can start a new project with ST MC Workbench software tool and upload the motor data directly inside.

"If you feel a post has answered your question, please click ""Accept as Solution"""
JEsca.1
JEsca.1Author
Associate II
March 25, 2020

Dear Cristiana, thanks for answer however my motor datasheet is not complete and profiler would be a good way to tune. I ordered F303 Nucleo to check only motor parameters. Thanks for your help.

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards