Skip to main content
KnarfB
Super User
March 6, 2019
Question

ST Motor Control Workbench failes to generate project with "Unable to deploy MotorControl reference pack"

I have installed MCSDK_v5.3.3 on my Win10 machine. I open example project P-NUCLEO-IHM001-BullRunning.stmcx, save it in a new folder as suggested and click the Generate icon.

The "Project generation" finds all my installed STM32CubeMX (4.27.0, 5.1.0), I select "ST SW4 STM32", "HAL", FW V1.10.0 (Recommended, not installed) and press the Generate button. Generation failes immediately saying:

"Deploying MotorControl Pack version `5.3.3` to D:\Users\Frank\Documents\STM32Cube\Repository\MCSDK_v5.3.3\MotorControl

Unable to deploy MotorControl reference pack to D:\Users\Frank\Documents\STM32Cube\Repository\MCSDK_v5.3.3\MotorControl

MotorControl reference pack not found: "../../../../Middlewares/ST/MotorControl"

Completed with errors"

Well, there is such a folder, but it is one "../" level off:

C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.3.3\Utilities\PC_Software\STMCWB>dir "../../../Middlewares/ST/MotorControl"

 Datenträger in Laufwerk C: ist Windows

 Volumeseriennummer: DAEE-B0E1

 Verzeichnis von C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.3.3\Middlewares\ST\MotorControl

06.03.2019 16:15   <DIR>         .

06.03.2019 16:15   <DIR>         ..

06.03.2019 16:15   <DIR>         lib

06.03.2019 16:15   <DIR>         MCSDK

21.01.2019 13:29           95.090 MotorControl_Configs.xml

21.01.2019 13:29          116.367 MotorControl_Modes.xml

21.01.2019 13:29           38.419 Release Notes for ST MC FOC FW.html

06.03.2019 16:15   <DIR>         templates

              3 Datei(en),       249.876 Bytes

When I change the Cube version etc., the error persists.

Am I missing someting? Can I change the folder?

Regards

Frank

This topic has been closed for replies.

3 replies

Claire O.
ST Employee
March 29, 2019

Dear Frank,

Please make sure you use the admin rights. If not, workbench will not be able to populate the repository in CubeMX folder.

Please tell me if it helps,

Thanks and best regards,

Claire

KnarfB
KnarfBAuthor
Super User
April 24, 2019

Yes, this works. Thanks.

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards