Skip to main content
omid hamdi
Associate III
Oct 28, 2019 6:24 AM UTC
Solved

st motor control library sdk v5.4 is possible control ac induction motor

in v2 st have ac motor control for ac induction on stm32f103 bou after this removed ac induction control how can fined v2 library or some sample code ac start document

in new v5.4 can support ac

in ac and pmsm motor only estimated rotor angle is different ?

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:45 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

2 replies

Laurent Ca...
Senior III
Jun 15, 2021 6:41 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:45 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards