Skip to main content
mscot.1
Associate II
July 22, 2020
Solved

ST MCW - MCSDK_v5.4.3 Bug? get compiler build error as PARK_ANGLE_COMPENSATION_FACTOR is not defined

On IAR & CubeIDE

For Sensorless configuration on a custom board.

This topic has been closed for replies.
Claire O.
Claire O.Best answer
ST Employee
July 23, 2020

ok, I can advise you to test with a ST board first , the one closest to your configuration.

The rational is that all ST boards available in the MCWorkbench have been tested by the ST team.

5 replies

Claire O.
ST Employee
July 23, 2020

Hello mscot.1,

Can you please describe a bit more your different steps?

Especially the custom board... did you use a known ST board to get started ?

Thanks,

Claire

mscot.1
mscot.1Author
Associate II
July 23, 2020

Hi Claire,

No I didn't, but if I try builds for Hall Sensors or Encoders are OK, that is they spin the motor via the Monitor etc.

Claire O.
Claire O.Best answer
ST Employee
July 23, 2020

ok, I can advise you to test with a ST board first , the one closest to your configuration.

The rational is that all ST boards available in the MCWorkbench have been tested by the ST team.

Luczia
Associate II
November 1, 2020

Hello,

I do have the same error with a nucleo f401RE and Ihm08-3Sh

In function 'FOC_CurrControllerM1':
C:/XXXXXX/Src/mc_tasks.c:770:50: error: 'PARK_ANGLE_COMPENSATION_FACTOR' undeclared (first use in this function); did you mean 'REV_PARK_ANGLE_COMPENSATION_FACTOR'?
 
 hElAngle += SPD_GetInstElSpeedDpp(speedHandle)*PARK_ANGLE_COMPENSATION_FACTOR;

It appears when unboxing hall sensors and quadrature encoder and activating Sensor-less (Observer+PLL) speed feedback.

STM32CubeMX 6.0.1

STM32 FW V1.25.1

STM32CubeIDE

DriveType : HAL

Visitor II
October 11, 2023

define PARK_ANGLE_COMPENSATION_FACTOR 0;