Associate III
Feb 25, 2024 8:32 PM UTC
Question
Speed ramp with Potentiometer
- 3 replies
- 2156 views
"I'm trying to rotate the motor using potentiometer libraries. Do you think there are any other missing parts that I need to determine?"
uint16_t potMeasArray[16];
potentiometerHandle.LPFilterBandwidthPOW2=4;
potentiometerHandle.PotMeasArray=potMeasArray;
potentiometerHandle.PotRegConvHandle=3;
potentiometerHandle.Valid=true;
POT_Init(&potentiometerHandle);
speedPotentiometerHandle.Pot =potentiometerHandle ;
speedPotentiometerHandle.pMCI = pMCI[M1];
speedPotentiometerHandle.RampSlope = 0.5;
speedPotentiometerHandle.ConversionFactor =88;
speedPotentiometerHandle.SpeedAdjustmentRange = 10;
speedPotentiometerHandle.MinimumSpeed =100;
speedPotentiometerHandle.LastSpeedRefSet = 650;
SPDPOT_Init(&speedPotentiometerHandle);