Skip to main content
Associate II
Sep 2, 2025 11:15 AM UTC
Question

Speed Feedback & Overvoltage Faults with Sensorless BLDC Motor (Nucleo-F101RE + X-Nucleo-IHM16M1)

Hello,

I am running a BLDC motor in sensorless mode using Nucleo-F101RE with the X-Nucleo-IHM16M1 board. The motor starts successfully when I press the Start button from the Motor Pilot GUI.

However, I am facing the following issues:

  • When I suddenly increase the speed to high RPM, I get a speed feedback fault.

  • When I suddenly decrease the speed, I also get a speed feedback fault.

  • Sometimes I also encounter an overvoltage fault during these speed changes.

Any guidance on how to resolve or tune the parameters properly would be very helpful.

Thank you

Best Regards

Rahul

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
Sep 2, 2025 1:34 PM UTC

Hello @Bablu,

For speed feedback fault, review 2.10. Why do I have a Speed feedback fault message chapter in Frequently Asked Questions link.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA