Skip to main content
Associate III
Aug 31, 2026 5:41 AM UTC
Question

Speed feedback error in sensorless foc at low RPM

While driving STM32303E-EVAL with STEVAL-IPM20B in sensorless (Observer +PLL) foc mode , speed feedback occurs at below 400 RPM and motor stops. 

1 reply

Visitor II
Aug 31, 2026 6:35 AM UTC

Your motor stops below 400 RPM because sensorless FOC with Observer + PLL loses reliable position estimation at very low speeds. The solution is to adjust startup/low‑speed parameters or use an encoder/Hall sensor for stable feedback.