Skip to main content
Associate II
Feb 12, 2025 12:56 PM UTC
Question

Speed Feedback error

Hello,

I am currently working with a custom board using an STGIB15CH60TS-LZ driver and an STM32H503RBT6 microcontroller.

The motor is a 48V, 500W, 300 RPM brushless motor with three Hall effect sensors (120° mechanical angle, 300° electrical angle). It is used in an electric bike.

I am using the FOC algorithm with:

  • Single shunt resistor
  • 16k PWM generation
  • Hall sensors as the main sensor

Everything works correctly, but I sometimes have an issue at startup and under load. Once the motor is running, the issue does not occur.

The image shows the three Hall effect sensors during a failed startup. In this case, the issue comes from the C2 signal.

I believe the problem is caused by small movements in the opposite direction of the expected motor rotation for the FOC algorithm. The motor controller returns a "speed feedback" error.

I am looking for a solution to prevent this error in the FOC algorithm since the reverse movements are unavoidable.

Thank you.

GetAttachmentThumbnail.jpg

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
Apr 22, 2025 1:13 PM UTC

Hello @Cedd,

Firstly, we would like to apologize for the delay in replying to your post.

Did you base your custom board on STEVAL-IPM15B board? If yes, did you check your HALL signals after the RC filtering?

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA