Associate II
May 17, 2022 7:16 AM UTC
Question
Sensorless FOC - sudden motor rotation change
- 5 replies
- 2010 views
Hi Community
I'm using the following setup:
- MC Motor Control Workbench v6.0.0
- STM32 FW V1.5.0 (HAL)
- Power + Control Board: B-G431B-ESC1
- Observer + PLL (Sensorless)
- Motor 10 pole pair
- Mech. Speed 200rpm
The motor starts and ramps up to 200rpm.
It can now happen that when there is a load change, the rotor suddenly turns at full speed in the opposite direction. The speed is displayed in the Motor Pilot. In this case, however, the phase current looks distorted.
What can be the cause?