Skip to main content
Associate III
May 5, 2025 1:05 AM UTC
Question

rev-up : on the fly star up

Hello Everybody,

MCSDK:6.3.0

CubeMX: 6.1.1

Workbench : 6.3.0

CubeIDE : 1.15.0

 

I’m currently working on a sensorless FOC setup using SMO + PLL for rotor angle estimation.
During the rev-up phase, I'm trying to implement on-the-fly startup, where the motor may already be rotating due to external force (like pedaling), and I want to bypass the full open-loop startup.

My question is:
What are the recommended conditions to ensure a safe and successful on-the-fly transition into torque mode?
For example:

Is there a minimum BEMF threshold (corresponding to a certain RPM) that must be exceeded to allow PLL to lock reliably?

Should I apply a delay or stability check to confirm the estimated angle and angular speed are stable before switching to torque mode?

Any suggestions for handling low-speed startup on uphill slopes, where the BEMF may be too weak for proper PLL locking?

Thank you in advance for any advice!

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
May 13, 2025 7:38 AM UTC

Hello @Vincent7,

You can refer to embedded On-The-Fly implementation:

GMA_0-1747121858691.png

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA