Skip to main content
NM_it
Associate III
Nov 25, 2020 2:52 PM UTC
Solved

Required Manual for ST Motor Control Workbench Serial Interface Protocol

Hi,

STM32 is working very well with the Windows application ST Motor Control Workbench Monitor. I want a interface document or manual for the serial communication which is happening between the STM32 and Control bench application. So that I can use the same communication protocol for master controller to interface with the BLDC driver controller instead of PC application.

Regards,

Nishanth M

This topic has been closed for replies.
AntoineC
AntoineCBest answer
ST Employee
Nov 30, 2020 9:14 AM UTC

Hello @NM​,

You can find in the section 14 - Serial communication class overview of the User Manual 1052 STM32F PMSM single/dual FOC SDK v4.3, a dedicated part for the explanation of the MCSDK communication protocol.

Best Regards,

Antoine

2 replies

AntoineC
AntoineCBest answer
ST Employee
Nov 30, 2020 9:14 AM UTC

Hello @NM​,

You can find in the section 14 - Serial communication class overview of the User Manual 1052 STM32F PMSM single/dual FOC SDK v4.3, a dedicated part for the explanation of the MCSDK communication protocol.

Best Regards,

Antoine

NM_it
NM_itAuthor
Associate III
Dec 1, 2020 5:52 AM UTC

Hi,

Thanks for your reply.... I got the document which I am looking for it.

Kind Regards,

Nishanth M