Skip to main content
Associate II
February 19, 2024
Solved

Red flashing light when I connect my B-G431B-ESC1 board

Hi there, 

I recently purchased the B-G431B-ESC1 and when I connect it to my USB port, immediately a red flashing light appears. There are two other solid green lights. 

I am also not able to connect my ST-LINK to flash firmware, and this may be related. But for that I am having issues installing the necessary drivers on my Windows10 laptop. 

I have downloaded the relevant drivers and upon installation I am told that they were installed successfully, yet when I launch Device Manager I am not able to see them anywhere. Furthermore, when I try to launch the ST-link utility software I am told it is unable to launch because of some missing DLL files, namely mfc140.dll, VCRUNTIME140.dll, and MSVCP140.dll. 

With a little online research on forums I see many suggesting I reinstall Visual C++ Redistributable. So I do that just (I remove what I had and installed Visual C++ Redistributable). But it did not help at all. 

Any help to get me started with this board would be most appreciated. I have the issue with ST-link drivers which I am hoping would resolve the red flashing LED, but something tells me they may not be related. 

Much appreciated. 

    This topic has been closed for replies.
    HudsonSamBest answer
    Associate II
    February 19, 2024

    Problem resolved: Turned out to be incorrect cables. I was (unknowingly) using power-only USB cables (i.e. no data) and hence the blinking RED light. 


    1 reply

    HudsonSamAuthorBest answer
    Associate II
    February 19, 2024

    Problem resolved: Turned out to be incorrect cables. I was (unknowingly) using power-only USB cables (i.e. no data) and hence the blinking RED light.