Re: How to generate profiler firmware for 6.2
- 15 replies
- 15476 views
Hi Zied,
After waiting patiently for MCSDK 6.2.0, I was overjoyed when it was finally released.
However, I could not get the motor profiler to communicate with my board. It seems to require a proper firmware to be downloaded before it can run. It does not allow me to select the correct boards even after the uart connection is done (although it instructed to "try to configure the board"). see attached screen grab.
[VERSION]: MCSDK 6.2.0
[TOOL]: Motor PROFILER v1.2.4
[DETAILS]: Not able to choose any control nor power board
[EXPECTED BEHAVIOR]: I could usually be able to select the boards and enter into "Start Profile"
I saw from other posting, your suggestion to download .hex into the board first and so I had tried to use NUCLEO-F302R8#X-NUCLEO-IHM08M1 3Sh#(6.1.2).hex from the MCSDK 6.2.0 folder. Once connected, it shows the boards, but I want to use CTM009v1, not IHM08M1. So, that is a problem. See attached 2nd screen grab.
Thirdly, I had also used the Workbench 6.2.0 to create a new project, select the right boards but unable to use my motor because no motor file is created yet (failed at Motor profiler).
Please help, I need to get this going but it has been delayed due to these configuration issues.
Thank you.
Regards,
Jedijump