Skip to main content
EDuat.1
Associate II
Nov 10, 2020 9:27 AM UTC
Solved

PWM Combined 3 Phase Mode, ADC Trigger, unexpected behaviour

Hi guys,

I am working on Motor Control and I need to set up Combined PWM and ADC trigger syncronize together.Last situation is PWMs working and ADC is trigered so when the ADC is triggered ,interrupt event is running in HAL_ADCEx_InjectedConvCpltCallback that I put in it Led Toggle what I see is trigger event is not runnning in every pwm period.Trigger event is running 1 time and no interrupt 2 times and again running interrupt.If I am gonna tell it in different way --> run wait wait run wait wait run ... Like that ,I am not sure drawing right but probably enough.Also HAL_TIM_TriggerCallback doesn't work.

_____-----_-----_______-----_-----_______-----_-----________-----_-----_______-----_-----___ PWM 1

____-------_-------____-------_-------____-------_-------_____-------_-------____-------_-------___ PWM 2

___--------_--------___--------_--------___--------_--------___--------_--------___--------_-------___ PWM 3

-------------______________________________________________----------------------------------- LED inside interrupt

Codes below

//----------------------- tim.c -----------------------//
#include "tim.h"
 
extern uint32_t timerPeriod;
 
TIM_HandleTypeDef htim1;
 
void MX_TIM1_Init(void)
{
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
 
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_CENTERALIGNED2;
 htim1.Init.Period = timerPeriod;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_OC5REF_RISING_OC6REF_FALLING;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 { Error_Handler(); }
 sConfigOC.Pulse = 0;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
 { Error_Handler(); }
 sConfigOC.Pulse = 0;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
 { Error_Handler(); }
 sConfigOC.OCMode = TIM_OCMODE_PWM2;
 sConfigOC.Pulse = 1000;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_5) != HAL_OK)
 { Error_Handler(); }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 200;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
 sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
 sBreakDeadTimeConfig.Break2Filter = 0;
 sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 { Error_Handler(); }
 HAL_TIM_MspPostInit(&htim1);
}
 
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{
 if(tim_baseHandle->Instance==TIM1)
 {
 __HAL_RCC_TIM1_CLK_ENABLE();
 HAL_NVIC_SetPriority(TIM1_UP_TIM16_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn);
 HAL_NVIC_SetPriority(TIM1_TRG_COM_TIM17_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM1_TRG_COM_TIM17_IRQn);
 }
}
void HAL_TIM_MspPostInit(TIM_HandleTypeDef* timHandle)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(timHandle->Instance==TIM1)
 {
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**TIM1 GPIO Configuration
 PA7 ------> TIM1_CH1N
 PB0 ------> TIM1_CH2N
 PB1 ------> TIM1_CH3N
 PA8 ------> TIM1_CH1
 PA9 ------> TIM1_CH2
 PA10 ------> TIM1_CH3
 */
 GPIO_InitStruct.Pin = PWM_UL_Pin|PWM_UH_Pin|PWM_VH_Pin|PWM_WH_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF6_TIM1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = PWM_VL_Pin|PWM_WL_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF6_TIM1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 }
}
 
//----------------------- main.c -----------------------//
 
int main(void)
{
 HAL_Init();
 SystemClock_Config();
 
 mcuFreq = HAL_RCC_GetSysClockFreq();
 timerPeriod = (uint32_t)((mcuFreq / 10000) - 1);
 
 MX_GPIO_Init();
 MX_TIM1_Init();
 MX_ADC1_Init();
 MX_USART1_UART_Init();
 
 __HAL_UART_FLUSH_DRREGISTER(&huart1);
 __HAL_TIM_ENABLE_IT(&htim1,TIM_IT_TRIGGER | TIM_IT_UPDATE);
 
 if(HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED) != HAL_OK); Error_Handler();
 HAL_ADCEx_InjectedStart_IT(&hadc1);
 
 valBuf[0] = setDutyPercentage(40);
 valBuf[1] = setDutyPercentage(50);
 valBuf[2] = setDutyPercentage(80);
 
 if(HAL_TIMEx_GroupChannel5(&htim1, (TIM_GROUPCH5_OC1REFC |\
 TIM_GROUPCH5_OC2REFC |\
 TIM_GROUPCH5_OC3REFC)) != HAL_OK)	Error_Handler();
 //if(HAL_TIMEx_GroupChannel5(&htim1, TIM_GROUPCH5_OC3REFC) != HAL_OK)	Error_Handler();
 
 if( HAL_TIM_Base_Start(&htim1) != HAL_OK )	Error_Handler();
 
 if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1) != HAL_OK) 	Error_Handler();
 if(HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_1) != HAL_OK)	Error_Handler();
 if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_2) != HAL_OK) 	Error_Handler();
 if(HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_2) != HAL_OK)	Error_Handler();
 if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_3) != HAL_OK) 	Error_Handler();
 if(HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_3) != HAL_OK)	Error_Handler();
 if(HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_5) != HAL_OK)		Error_Handler(); //ADC Trigger
 
 
 TIM1->CCR1 = valBuf[0];
 TIM1->CCR2 = valBuf[1];
 TIM1->CCR3 = valBuf[2];
 
 HAL_UART_Receive_IT(&huart1, uartRxBuf, 1);
 
 while (1)
 {
	 u16TimerVal = __HAL_TIM_GET_COUNTER(&htim1);
 }
}
 
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);
 
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV6;
 RCC_OscInitStruct.PLL.PLLN = 85;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 { Error_Handler(); }
 
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {Error_Handler(); }
 
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_ADC12;
 PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
 PeriphClkInit.Adc12ClockSelection = RCC_ADC12CLKSOURCE_SYSCLK;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {Error_Handler(); }
}
 
uint32_t setDutyPercentage(uint32_t val)
{
	return (( val * (timerPeriod - 1)) / 100);
}
 
void HAL_ADCEx_InjectedConvCpltCallback(ADC_HandleTypeDef *hadc)
{
	ADConvertedValues[2] = HAL_ADCEx_InjectedGetValue(&hadc1, ADC_INJECTED_RANK_3);
	HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
}
 
//This interrupt doesn't work
void HAL_TIM_TriggerCallback(TIM_HandleTypeDef *htim)
{
	//HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
	__HAL_TIM_CLEAR_FLAG(&htim1,TIM_IT_TRIGGER);
}

This topic has been closed for replies.
EDuat.1
EDuat.1Best answer
Associate II
Nov 12, 2020 11:04 AM UTC

Solved.Because of discontinuous mode

2 replies

EDuat.1
EDuat.1AuthorBest answer
Associate II
Nov 12, 2020 11:04 AM UTC

Solved.Because of discontinuous mode

Laurent Ca...
Senior III
Nov 19, 2020 9:19 AM UTC

Dear @Community member​ 

Happy for you.

Feel free to ask any other questions you want.

Best regards

Laurent Ca...