Skip to main content
KWikt.1
Visitor II
January 31, 2020
Question

Problem with encoders on Nucleo-446RE.

Hello!

Im working at inspecting vechicle. It is made of nucleo-446re, DRV8835 motor driver, two DC motors and two optical encoders mounted on motros. The encoders are manufactured by Pololu. First encoder is conected to TIM3 CH1 and CH2 on pins PA6 and PA7. The second is conected to TIM2 CH1 and CH2 on pins PA5 and PB3.

The problem is that the motors run at the same speed but one encoder on TIM3 faster read impulses.

Im working with STM32CubeMX and STM32CubeIDE. Also im using STM Studio to check impulses on both motors.

My code snippets:

static void MX_TIM2_Init(void)
{
 TIM_Encoder_InitTypeDef sConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 65535;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 sConfig.EncoderMode = TIM_ENCODERMODE_TI12;
 sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC1Filter = 15;
 sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC2Filter = 15;
 if (HAL_TIM_Encoder_Init(&htim2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
}
static void MX_TIM3_Init(void)
{
 TIM_Encoder_InitTypeDef sConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 0;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 65535;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 sConfig.EncoderMode = TIM_ENCODERMODE_TI12;
 sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC1Filter = 15;
 sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC2Filter = 15;
 if (HAL_TIM_Encoder_Init(&htim3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
}
while(1){
 encoder1_counter = TIM2->CNT;
 encoder2_counter = TIM3->CNT;
 HAL_Delay(10);
}

Regards KW.

This topic has been closed for replies.

2 replies

Laurent Ca...
Senior III
September 11, 2020

Dear KWikt.1

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
September 23, 2020

Dear @KWikt.1​ 

I guess you don't have to solve this problem anymore, therefore I consider this post closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...