Skip to main content
JHenn.2
Associate
Oct 21, 2020 4:39 PM UTC
Solved

Problem to Flash STEVAL SPIN 3201 Board Example

Hello,

I have a STEVAL-SPIN3201 board Rev 3.

Try to use the flash procedure from document UM2152

  • USB Connection to Windows 10 PC
  • 12V Power Supply to J2
  • Flash drive shows up with two files Fail.txt and Details.txt
  • I am able to delete the two files.
  • Windows shows a free memory of 24kB.
  • 12kB are always used.
  • Try to copy the SDK5x - STEVAL-SPIN3201 - BullRunning.bin example.
  • Windows refuses to copy because of insufficient space.

Is there any procedure to get the 12kB free?

Thanks in advance and best regards

Jens

This topic has been closed for replies.
JHenn.2
JHenn.2Best answer
Associate
Oct 21, 2020 7:07 PM UTC

I found the problem... I had to update the STLINK SW on the board. This can be done with the STM32cubeProgrammer SW

2 replies

JHenn.2
JHenn.2AuthorBest answer
Associate
Oct 21, 2020 7:07 PM UTC

I found the problem... I had to update the STLINK SW on the board. This can be done with the STM32cubeProgrammer SW

Laurent Ca...
Senior III
Oct 21, 2020 7:24 PM UTC

Dear @JHenn.2​ 

But you are welcome =) !

Best regards

Laurent Ca...