Skip to main content
DAlvarez
Associate II
October 7, 2022
Question

pin level when disabling pwm

I'm using a general-purpose timer to generate low level pulses, configuring one channel as PWM. The problem is when I disable the channel, the signal goes low, and I want it to remain high.

I played with the OCPolarity and PWM modes 1 and 2, but only take effect when the PWM is running, when disabling the pin always goes low

any suggestion?

MCU STM32F722ZETx (Nucleo F722ZE)

main

 LL_TIM_EnableCounter(TIM9);
 bool active_inactive = false;
 while (1) {
 if (HAL_GPIO_ReadPin(USER_Btn_GPIO_Port, USER_Btn_Pin) == GPIO_PIN_SET){
 while(HAL_GPIO_ReadPin(USER_Btn_GPIO_Port, USER_Btn_Pin) == GPIO_PIN_SET);
 if(active_inactive){
 LL_TIM_CC_EnableChannel(TIM9, LL_TIM_CHANNEL_CH1);
 LL_TIM_ClearFlag_UPDATE(TIM9);
 LL_TIM_EnableIT_UPDATE(TIM9);
 }
 else{
 LL_TIM_DisableIT_UPDATE(TIM9);
 LL_TIM_CC_DisableChannel(TIM9, LL_TIM_CHANNEL_CH1);
 }
 active_inactive = !active_inactive;
 HAL_Delay(50);
 }
 HAL_Delay(1);
 }

Configuration generated by cubeMX

/**
 * @brief TIM9 Initialization Function
 * @param None
 * @retval None
 */
static void MX_TIM9_Init(void)
{
 
 /* USER CODE BEGIN TIM9_Init 0 */
 
 /* USER CODE END TIM9_Init 0 */
 
 LL_TIM_InitTypeDef TIM_InitStruct = {0};
 LL_TIM_OC_InitTypeDef TIM_OC_InitStruct = {0};
 
 LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* Peripheral clock enable */
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_TIM9);
 
 /* TIM9 interrupt Init */
 NVIC_SetPriority(TIM1_BRK_TIM9_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
 NVIC_EnableIRQ(TIM1_BRK_TIM9_IRQn);
 
 /* USER CODE BEGIN TIM9_Init 1 */
 
 /* USER CODE END TIM9_Init 1 */
 TIM_InitStruct.Prescaler = 0;
 TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
 TIM_InitStruct.Autoreload = 647;
 TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;
 LL_TIM_Init(TIM9, &TIM_InitStruct);
 LL_TIM_DisableARRPreload(TIM9);
 LL_TIM_SetClockSource(TIM9, LL_TIM_CLOCKSOURCE_INTERNAL);
 LL_TIM_OC_EnablePreload(TIM9, LL_TIM_CHANNEL_CH1);
 TIM_OC_InitStruct.OCMode = LL_TIM_OCMODE_PWM2;
 TIM_OC_InitStruct.OCState = LL_TIM_OCSTATE_DISABLE;
 TIM_OC_InitStruct.OCNState = LL_TIM_OCSTATE_DISABLE;
 TIM_OC_InitStruct.CompareValue = 5;
 TIM_OC_InitStruct.OCPolarity = LL_TIM_OCPOLARITY_HIGH;
 LL_TIM_OC_Init(TIM9, LL_TIM_CHANNEL_CH1, &TIM_OC_InitStruct);
 LL_TIM_OC_EnableFast(TIM9, LL_TIM_CHANNEL_CH1);
 /* USER CODE BEGIN TIM9_Init 2 */
 
 /* USER CODE END TIM9_Init 2 */
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOE);
 /**TIM9 GPIO Configuration
 PE5 ------> TIM9_CH1
 */
 GPIO_InitStruct.Pin = LL_GPIO_PIN_5;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct.Alternate = LL_GPIO_AF_3;
 LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
 
}

This topic has been closed for replies.

4 replies

Javier1
Principal
October 7, 2022

this is a common problem when implementing six steps trapezoidal control for BLDC motors.

If my memory doesnt fail me i ended up doing something like @Antypas.Peter​ said here https://community.st.com/s/question/0D50X00009sW6qlSAC/hal-pwm-stop-with-defined-pin-output

hit me up in https://www.linkedin.com/in/javiermuñoz/
AScha.3
Super User
October 7, 2022

set CH idle state - then you get hi idle

in cube:

0693W00000UnakSQAR.pngmaybe you need setting in break also:

0693W00000Unal1QAB.png...enable off state sel.

If you feel a post has answered your question, please click on " Best Answer ".
waclawek.jan
Super User
October 7, 2022

Or just switch the given pin to GPIO Out with whatever level you want.

[EDIT] Oh that's the same what Javier suggested above. [/EDIT]

JW

DAlvarez
DAlvarezAuthor
Associate II
October 10, 2022

Thanks for the answers. What @AScha.3​ suggests is only for advance timers and I'm using a general purpose one (I'm regrating this, but the PCB is already made)

So I will reconfigure the pin as gpio output and change the level before stopping the timer. Thanks again.