Skip to main content
Visitor II
May 20, 2026 1:32 PM UTC
Question

P-NUCLEO-IHM03 giving driver protection fault

Good evening, I am trying to use a P-NUCLEO-IHM03 pack.

giulioTam_0-1779283331625.png

I have generated the project using the X-CUBE-MCSDK version 6.4.2 and STM32cubeMX version 6.17.0, built and flashed the project on the board. The problem is that as soon as I try to start the motor in ST motor pilot, I get a driver protection fault instantly, without any movements of the motor:

giulioTam_1-1779283649343.png

I didn't touch any configuration and jumper of the board, but while I generate the project I get these warnings (I don't know if this coukd be the reason of the fault):
Screenshot 2026-05-20 152342.png

giulioTam_2-1779283920065.jpeg

Any help would be very much appreciated, Thanks.

 

1 reply

GMA
ST Technical Moderator
May 21, 2026 7:09 AM UTC

Hello @giulioTam,

Verify that both boards are connected correctly.
Refer to section 4.1 operation mode and sensing topology selection in the X-NUCLEO-IHM16M1 user manual for FOC 3-shunt board settings.
Warning messages relate to X-NUCLEO-IHM16M1 signal connections. For more details, refer to the board schematic available in the user manual. These warning messages can be ignored in the P-NUCLEO-IHM03 use case.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA