Skip to main content
Su XuanXian
Visitor II
May 24, 2017
Question

Over-current protection section

Posted on May 24, 2017 at 07:57

Hello, All:

I use (ST Motor control Workbench) parameters in power management where I set up some flow parameters, and then generate the file in Power stage, But  I did not find the parameters.h file to set my  parameters, why, where is it?

/*********** Over-current protection section ************/

#define OVERCURR_FEEDBACK_POLARITY EMSTOP2_ACTIVE_LOW

#define OVERCURR_PROTECTION_HW_DISABLING DOUT_ACTIVE_HIGH

/************************************************* ************/

There is no parameter about overcurrent.

Thank you!

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards