Skip to main content
Fkadr.1
Associate II
November 12, 2020
Question

Over current error evspin32f0

Hi

I have designed a board based on evspin32f0602 single shunt foc.

When I am using the same value of ​shunt resistor as the event spin board the motor runs normally

But I want to increase the load capacity to 16 amps

So what all changes i need to do beside shunt resistor. I have used .025 ohm as shunt resistor .

But now every time I turn on the motor it shows over load.

Is there any other resistor i have to change.​

Thanks.​

This topic has been closed for replies.

5 replies

PBo
Visitor II
November 24, 2020

Hello Fkadr.1,

The original EVSPIN32F0602S1 board is limited to 8.5 Apeak.

In its User's Manual (UM2629), it provides you with chapter 6.3 on How To modify HW about the Overcurrent detection and Current sensing measurement. In particular, it informs about the few resistors to change according to the given formula.

Then, you have to make sure that your FW configuration is matching this new HW configuration. The MC Workbench software tools will help you to do that (Cf. the Current Sensing and the  Overcurrent Protection blocks).

Best Regards.

Fkadr.1
Fkadr.1Author
Associate II
May 9, 2021

I have solved all my queries and​ made my own board with higher amp rating.

thanks for your response

Karan 123
Senior
May 9, 2021

Hi,

@Fkadr.1 , @PBo (ST Employee)

I have ordered EVSPIN32F0601S3 eval board but not received yet

Do I need only Enter Motor Parameters as in mcsdk 5.4.6 to spin the Motor (As parameters attached) ?

--

Karan

Fkadr.1
Fkadr.1Author
Associate II
May 9, 2021

This is all you will need to operate the motor.But once you start playing with the software you will be accurately operate motor.

Karan 123
Senior
May 9, 2021

Many of Thanks for update...

@Fkadr.1 (Community Member)

1) Means these 10 parameters (as attached) is sufficient to spin the motor ? Rest should be default in mcsdk 5.4.6 ?

2) How to choose PWM Frequency and Execution Rate ? According to Motor Parameter ?

0693W00000ANmi7QAD.png 

Any other suggestions ...

--

Karan