Skip to main content
Visitor II
Dec 3, 2025 2:22 AM UTC
Question

Operating the STEVAL-ESC002V1 with 8S battery?

I am curious what dictates the operating conditions of the STEVAL-ESC002V1 to a 2-6S battery and 20A current capability? I would like to use this chipset and operate from an 8S battery. The specs state that the MCU is capable of operating up to 45V and a fully charged 8S battery would only be 33.6V. Therefore I would assume the MCU can operate at the voltages I need and what would need to change on the EVAL board to test at the increased voltages?

1 reply

GMA
ST Technical Moderator
Dec 5, 2025 10:10 AM UTC

Hello @hoser,

From operating voltage range perspective, the board can be used with 8S battery packs, but load transients can cause overshoots on the supply.
We applied a 50% margin on the maximum battery voltage to take them into account, so the 8S batteries were excluded from the recommended range.

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA