Skip to main content
TKara.2
Associate III
October 21, 2024
Solved

Open loop control with potentiometer feature

 

Is it possible to change the starting direction in open-loop control? Can I adjust the initial parameters based on the potentiometer value? Where can I configure this?

TKara2_0-1729538129145.pngTKara2_1-1729538134902.png

 

    This topic has been closed for replies.
    Gael A
    Gael ABest answer
    ST Employee
    October 22, 2024

    Hello TKara.2,

    You can easily revert the starting direction by inputting a negative Speed Reference value to your command (both on Pilot and via APIs). Also, simply inverting two motor phases works.

    Concerning the Potentiometer, I'm afraid this feature is only meant to be used in Closed Loop, but you can take it as a starting point to implement an open loop version yourself.

    If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

    1 reply

    Gael A
    Gael ABest answer
    ST Employee
    October 22, 2024

    Hello TKara.2,

    You can easily revert the starting direction by inputting a negative Speed Reference value to your command (both on Pilot and via APIs). Also, simply inverting two motor phases works.

    Concerning the Potentiometer, I'm afraid this feature is only meant to be used in Closed Loop, but you can take it as a starting point to implement an open loop version yourself.

    If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.