Skip to main content
SDall
Associate III
February 10, 2022
Question

Odrive motor

hi i'm using a F401RE and a hmi016m1, using a brushless odrive motor, i'm using sdk notor control, i set motor type bull ranning, i left everything default the rest, but when i go to give the motor.start, the motor doesn't moves but makes a strange noise! what can i change?

This topic has been closed for replies.

23 replies

GMA
ST Technical Moderator
March 8, 2022

I don't catch your point. What do you mean by "it moves in deceleration"? Are you able to make the motor spinning or not?! Do you have an error reported to Motor pilot?

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
SDall
SDallAuthor
Associate III
March 8, 2022

no sorry now I was able to set the software correctly, now I understand how it works! my question now is how to spin it slowly, i need the rotor to move 90 degrees or 180 degrees, my specific use was for using a robotic arm!

GMA
ST Technical Moderator
March 9, 2022

For this kind of application, using motor with encoder and "Position control" set in "Drive Setting"/"Control mode" is the best solution. On Motor Pilot side load GUI "PositionControlApp.qml" file. This interface allows to set an angle "Target Position" and a "Duration".

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA