Nucleo power supply when plugged on X-NUCLEO-IHM08M1
Hello,
I am using an X-NUCLEO-IHM08M1 board plugged on a G431 Nucleo board and I have a question regarding the Nucleo power supply.
In the IHM08 Quick Start Guide it is noted that the JP5 PWR jumper must be set to E5V (powered from morpho connector), however in the Motor Profiler information page (when you click on "Remember to properly configure the boards in Motor Control Mode" - Step 1) it is 5V_STLK that is mentioned (powered from USB).
Which one should be used?
Also, is is recommended to use an "external Isolated ST LinkConnect", highlighting the Nucleo STLINK USB connector. What is this device? (the new B-STLINK-ISOL?)
Thank you.