Skip to main content
MKOTE.1
Associate
Apr 3, 2020 10:25 AM UTC
Solved

Nucleo-F302R8 : USB drivers installed, jumpers configuration done, but when I connect to the PC the LED LD2 remains OFF, LD1 blinks in red, LD3 red, and the PC don't see the device (No ST-link detected). Otherwise the board is working and the motor s

This topic has been closed for replies.
MKOTE.1
MKOTE.1Best answer
Associate
Oct 15, 2020 5:25 PM UTC

Dear Laurent,

The problem was in the USB cable that transmitted power but no data.

I changed the cable and it is working now.

Btw, it would be a good idea to provide the cable with the board!

Best regards,

Mohamad

6 replies

Claire O.
ST Employee
Apr 3, 2020 12:21 PM UTC

Hello MKOTE.1,

Can you please specify which SW you are using?

Thanks and best regards,

Claire

MKOTE.1
MKOTE.1Author
Associate
Apr 9, 2020 7:59 PM UTC

Hello Claire,

I tried with Motor Profiler, STM32 ST-LINK Utility, ST MC Workbench, EWARM, etc.

This is the first time I use the board, I've never seen the LED LD2 blinking.

Thanks,

Mohamad

MKOTE.1
MKOTE.1Author
Associate
Apr 3, 2020 4:54 PM UTC

Hello Claire,

I tried with Motor Profiler, STM32 ST-LINK Utility, ST MC Workbench, EWARM, etc.

This is the first time I use the board, I've never seen the LED LD2 blinking.

Thanks,

Mohamad

MKOTE.1
MKOTE.1Author
Associate
Apr 15, 2020 4:48 PM UTC

Any other suggestions? I need to be able to program the board.

Laurent Ca...
Senior III
Oct 15, 2020 9:43 AM UTC

Dear @MKOTE.1​ 

Do you have still this problem to solve?

If not, do not hesitate to share the final solution you found.

Best regards

Laurent Ca...

MKOTE.1
MKOTE.1AuthorBest answer
Associate
Oct 15, 2020 5:25 PM UTC

Dear Laurent,

The problem was in the USB cable that transmitted power but no data.

I changed the cable and it is working now.

Btw, it would be a good idea to provide the cable with the board!

Best regards,

Mohamad