Skip to main content
Associate
July 22, 2024
Question

Not possible to create motor control project with FOC with custom power board

I am unable to create motor control project with FOC algorithm using custom power. It generates an error:

It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the following mandatory features:
- Current Sensing

For more details, please, look at the following log file in your home directory: .st_workbench/connectAlgo.log

Although I've added current sensing and the report generated is fine.

Not sure what I'm doing wrong. I've also attached the log file.

This topic has been closed for replies.

6 replies

GMA
ST Technical Moderator
July 23, 2024

Hello @pranz-24,

Is-it possible to share your power board .json file? 
What is your use-case control board? 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
pranz-24Author
Associate
July 23, 2024

Sure

The control board I am using is STM32G431RB. (You can also try with STM32G474RE)

GMA
ST Technical Moderator
July 24, 2024

Hello @pranz-24,

If you do not intend to use HSO (High Sensitivity Observer) feature speed sensormode, you have to use TwoICSCurrents variant (check "3.1.3.1. Two ICS currents hardware variant" chapter in stwiki page and described in User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab>"Current sampling", "Current sampling in isolated current sensor topology" link.

For HSO purpose, you have to also define PhaseVoltageSensing feature variant in addition of ThreeICSCurrents variant.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA