Skip to main content
Associate II
Oct 10, 2025 12:51 PM UTC
Question

Not able to add custom motor in Motor control workbench 6.4.1

I want to add a custom motor under "New_Project" in MC Workbench. As soon as i am clonign previous motors, i am not able to edit it and the edit window is getting closed automatically.

Please suggest me what i should do.

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
Oct 13, 2025 7:22 AM UTC

Hello @Sanchari,

Using new project on Workbench 6.4.1 and clone motor, it is possible to edit motor parameters.

GMA_0-1760339864837.png

You can also edit the previous motor .json file (located in ~\.st_workbench\hardware\motor) using a text editor.

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA