Skip to main content
LRowi.1
Associate
August 26, 2021
Question

My STEVAL HKI001V2 is not able to communicate with SDK 5.Y.1 and SDK 5.Y.2 It can communicate with SDK 5,4,6 , What is a reason I am also not able to find the STEVAL HKI001V2board set on the Motor profiler list of boards Is this board set supported?

..

This topic has been closed for replies.

13 replies

LRowi.1
LRowi.1Author
Associate
October 19, 2021

Hello again.

Thank you very much for the explanation. Following your advice I try to go through the example using the Keil MDA IDE software. However please clarify how the the Steval set can be configured for 400 A motor while it is provided with the ACEPACK™ 2 bridge with 35 A capacity. I can also see no difference in example project configuration while compared to configuration available as the new project loaded from the Workbench (except for motor data)

Best regards

****

cedric H
ST Technical Moderator
October 20, 2021

Hello @LRowi.1​,

From https://www.st.com/en/evaluation-tools/steval-hki001v2.html, this board supports up to 35 A. Where did you see that it can be configured for a 400 A motor ?

The difference in the example project is around the configuration of the BKIN pin.

Regards

Cedric