Skip to main content
OMarc.1
Associate II
December 15, 2021
Question

MotorControl Workbench generate project with 20+ errors in STMCUBEIDE

STM Motor Workbench

When I tested the motor in Motor Profiler, I am adding the settings to MotorControl Workbench, and generated the project in CubeMx, but when I try to compile the program I have 20+ errors like:

undefined reference to `STO_PLL_Init'

undefined reference to `RUC_Init'

in question (https://community.st.com/s/question/0D50X00009XkWF5/motor-control-sdk-510-and-sw4stm32-not-compiling) was the same problem, but the solution didn't work, I think I didn't know how to add a library in STMCUBE_IDE right, maybe it's a problem.

Board: Nucleo-F303RE + IHM16M13S

Soft: STMCUBE_IDE 1.8.0

Motor Workcbench 5.4.8

This topic has been closed for replies.

2 replies

Laurent Ca...
Senior III
December 21, 2021

Dear @OMarc.1​ 

Sorry for the late answer.

Do you have still this problem to solve?

And just in case, if not, do not hesitate to share the final solution you found. Thanks by advance.

Best regards

OMarc.1
OMarc.1Author
Associate II
December 21, 2021

I thought you would share the solution with me.

Yes, the problem exists and it is connected only with CubeIDE.

Kind regards.