Skip to main content
Kse.1
Associate
Feb 18, 2025 6:57 AM UTC
Solved

MotorControl Workbench_6.3.2 __weak void MX_MotorControl_Init() ... can be excuetable??

 

1. using Workbench

"B-G431B-ESC1" board, "Gimbal GBM2804H-100T" motor

2. Generated Code "stm32CubeIDE", drive type: HAL

 

3. CubeIde code.

generated code as below...........

in main(), MX_MotorControl_Init() function can be executable normally?

Shouldn't the "__weak" in front of the function disappear?

Is the code generated properly?

Is there something wrong with the setting?

I generated the code without connecting B-G431B-ESC1.

 

 

main.c
int main(void)
{

..........
MX_TIM2_Init();
MX_MotorControl_Init();

/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}

 

 

motorcontrol.c

 

__weak void MX_MotorControl_Init(void)

{

/* Reconfigure the SysTick interrupt to fire every 500 us. */

(void)HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq() / SYS_TICK_FREQUENCY);

HAL_NVIC_SetPriority(SysTick_IRQn, uwTickPrio, 0U);

 

/* Initialize the Motor Control Subsystem */

MCboot(pMCI);

mc_lock_pins();

}

 

 

mc_task.c

__weak void MCboot( MCI_Handle_t* pMCIList[NBR_OF_MOTORS] )

{.........}

 

__weak void mc_lock_pins (void)

{.........}

 

 

 

 

........Thank you in advance.

This topic has been closed for replies.
Kse.1
Kse.1Best answer
Associate
Feb 20, 2025 1:14 AM UTC


I didn't get it right.
The problem has been resolved.

 

filex.h 

     void A();

 

filex.c

__weak void A()

{

   printf("abc");

}

 

main.c

int main()

{

   A();

}

 

result:   abc  ... normally printed


If  A()  is not defined in another file in main.c:
An A() call defined in filex.c is called "abc".

2 replies

GMA
ST Technical Moderator
Feb 19, 2025 8:37 AM UTC

Hello @Kse.1,
- What do you mean by "in main(), MX_MotorControl_Init() function can be executable normally?"?
- Code generation status is visible on "Project generation" window.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Kse.1
Kse.1AuthorBest answer
Associate
Feb 20, 2025 1:14 AM UTC


I didn't get it right.
The problem has been resolved.

 

filex.h 

     void A();

 

filex.c

__weak void A()

{

   printf("abc");

}

 

main.c

int main()

{

   A();

}

 

result:   abc  ... normally printed


If  A()  is not defined in another file in main.c:
An A() call defined in filex.c is called "abc".