Visitor II
March 22, 2021
Question
MotorControl Workbench 5.4.4 Position control
- 2 replies
- 3249 views
Hello everyone
I want to use MotorControl Workbench 5.4.4 to generate a position control program with a Z-phase index signal, but MotorControl Workbench 5.4.4 does not have the pins in my hardware, only PB10 and PB2, the pins corresponding to my Z-phase index signal It is PE6. When I download the corresponding program to the board after completing the corresponding operation according to the AN5464 note, the motor will not find the position of the Z-phase index signal, and there are some problems with other functions. Ask everyone, what should I do next?
Thank you