Associate II
May 20, 2025 9:50 AM UTC
Question
Motor startup failure error
- 5 replies
- 846 views
Dear Support team,
I am currently working on a sensorless motor control application using the Observer + PLL algorithm to run a 24V PMSM motor (rated at 3600 RPM, no load) on a custom driver board based on the STM32F030R8. My PWM frequency is 8000kHz and I am using a single shunt resistor for current sensing.
The motor appears to operate correctly during the ramp-up phase. However, it stops immediately after transitioning to closed-loop FOC, triggering a startup failure error.
I am using STM32 Motor Control Workbench version 5.4.8 for configuration. I have attached the wb file and .stmcx file in .txt format containing the full GUI-based configurations for your reference.
I would appreciate your assistance in resolving this issue.