Motor profiler MCSDK 6.2.0
- 2 replies
- 1665 views
I am moving to MCSDK 6.2.0 and want to test the motor profiler new feature.
[VERSION]: MCSDK 6.2.0
[TOOL]: Motor PROFILER v1.2.4
EVALSTDRIVE101 + NUCLEO-F746ZG + Custom board for adapter
[DETAILS]: Fail to do motor profiling
[EXPECTED BEHAVIOR]: Able to do motor profiling even with custom board
Attached is the project
The resistorOffset is not defined for the EVALSTDRIVE101, so I first do the offset detection. Measured value is approximatly the know motor resistor and resistor offset is therefore negative.
Then I start profiling the motor but stay stuck with the message to increase (or decrease) the max speed. I have tried different value without success.
I know that this Power board is not listed in the table 2 (list of described boards containing resistorOffset parameter) in the motor profile page. And this board combo was not compatible with motor profiler in the past. But should I expect to work with MCSDK 6.2.0 ?
When I am injected the motor known information from my 6.1.2 project, it does not work straight out of the box. But for this point I need to investigate a bit more.
Thanks.