Skip to main content
Associate
Jun 5, 2025 9:38 AM UTC
Solved

Motor profiler error using B-G431B-ESC1

I try to do the motor drive using a B-G431B-ESC1 board.

When I connect the board, the following warning appeared.

  • [WARNING] - MotorControlRegistersBank: Accessing register [7449] RESISTOR_OFFSET resulted in error[5] . Changing register's access accordingly to avoid getting this error again

The software version is  V6.4.0.

I could obtain the electrical and mechanical models by clicking "start profile" after the motor connected to the motor driver rotated.

But, in the "register" tab, the status of register [7449] is "error".

Could you please tell me how to solve this error?

Thanks.

This topic has been closed for replies.
GMA
GMABest answer
ST Technical Moderator
Jun 6, 2025 4:08 PM UTC

Hello @Saka,

The hex files located in ".../STM32CubeProgrammer/Fw" directory have been generated for MCSDK6.1.2 and are not relevant for MCSDK6.4.0 (will be removed on next MC Motor Pilot tool deliveries, thank you for the report).
For MCSDK6.4.0 version, refer to User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab, "Motor Profiler Application Note" link for Motor Profiler project generation and usage.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

7 replies

GMA
ST Technical Moderator
Jun 5, 2025 3:15 PM UTC

Hello,

Using MCSDK6.4.0 B-G431B-ESC1 Motor Profiler use case from scratch; I do not have such error.
Do you use the associated Motor Pilot 6.4.0 tool? 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
SakaAuthor
Associate
Jun 5, 2025 11:56 PM UTC

I use the Motor Pilot 6.4.0 tool.

Before the running, I used the STM32CubeProgrammer and programed the hex file named "B-G431B-ESC1#B-G431B-ESC1 3Sh#(6.1.2).hex".

GMA
ST Technical Moderator
Jun 6, 2025 7:29 AM UTC

Hello @Saka,

Is your hex file generated with MCSDK6.1.2? If yes, regenerating the project with MCSDK6.4.0 should solve the problem.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA