Skip to main content
HLewo
Visitor II
February 19, 2019
Question

Motor profiler and delta connected windings

  • February 19, 2019
  • 1 reply
  • 566 views

In all fan motors that we like to profile the three windings are delta connected.

The motor profiler runs but states at the end that the resistances and inductivities are out of the range of supported values. Is there a possibility to switch the behavior of the motor profiler to profile delta connected motors? And furthermore are the software libraries that drive the motor able to drive delta connected motors?

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards