Skip to main content
KToo.1
Visitor II
September 12, 2022
Question

Motor Profiler 5.4.8 and Maximum Speed

Hi,

I am using motor profiler 5.4.8 with F302R8 and IHM08M1 to get the motor profile of my BLDC motor.

I have a query. Let say the maximum speed i get from the motor profiler is 30krpm. Can i change the maximum speed in motor control workbench (e.g. from 30krpm to 40krpm) and adjust the motor speed up to 40krpm in workbench?

Thanks,

Kim

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
October 12, 2022

Hello,

Have you set 40krpm on "Max Speed" profiler interface before profiling the motor?

If yes, and if profiler provides a lower max speed than expected, may be that electrical parameters, as Vbus value e.g., have be increased...

On the other hand, yes, you can change the "Max. Application speed" clicking motor "M" on workbench interface.

Best regards.

GMA

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA