Skip to main content
omid hamdi
Associate III
July 9, 2021
Question

motor profiler

when used custom board how to used motor profiler for detect motor parameter

motor parameter calculated in stm32 or in motor control profiler

This topic has been closed for replies.

3 replies

cedric H
ST Technical Moderator
July 9, 2021

Hello,

For the time being, the motor profiler can be used only on the ST boards proposed by the tool.

Regards

Cedric

omid hamdi
Associate III
July 9, 2021

calculated motor parameter in stm32 ic or in side motor control profiler

cedric H
ST Technical Moderator
July 9, 2021

The motor parameters are computed by the MCU with a dedicated firmware. This firmware is generated for all proposed boards it is why it is not open yet to custom boards. The PC tool is not involved in the parameters detection.