Skip to main content
nmamore
Associate II
August 10, 2021
Question

Motor occasionally spins much faster than commanded

Unfortunately, I do not have much info as to what causes this. I am using the FOC library with a 3-phase BLDC and encoder as speed feedback. Sometimes when I send a ramp command, the motor flies to ~5000 RPM regardless of the target speed I set. It is very infrequent. It can be fixed by cycling power it seems. Anyone run into similar issue?

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
September 5, 2021

Dear @nmamore​ 

We need more data to help you (configurations, pictures, screenshots, etc.).

Is it possible?

Best regards