Skip to main content
Associate
April 9, 2025
Question

Motor Not Starting with Encoder – Works Fine in Sensorless Mode

Good day,

First, a bit about my hardware:
Motor:

  • 4 pole pairs

  • 24V

  • Max speed: 3080 rpm

Inverter board:

  • B-G431B-ESC1

  • External power supply via power adapter

Encoder:

  • 490-AMT10E2-V set to 640 PPR

Now to my problem:

When I start the motor in sensorless mode, everything works as expected.
However, as soon as I use the encoder, it stops working — the motor just twitches briefly. In Motor Pilot, it briefly switches to "alignment" but immediately falls back to "idle."

In the plot, I’m monitoring the ENCODER_EL_ANGLE, which moves smoothly between -180 and +180 degrees without any noticeable jumps if i turn it by hand.

I also tried setting the encoder as an auxiliary sensor just to observe it while the motor is running, but even then, the motor doesn't work — same behavior as described above.

I’ve read the encoder data using my own code, and it works even at higher speeds.

Changing the encoder direction or adjusting the alignment current and time didn’t help either.

Does anyone have any idea what could be wrong?

Thanks in advance!

This topic has been closed for replies.

4 replies

GMA
ST Technical Moderator
April 11, 2025

Hello @FZTHUB,

Using Main Speed Sensor in sensor less mode, and auxiliary Speed Sensor in encoder mode, motor does not spin?
If motor is able to spin, are the two electrical angle signals in phase?

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
FZTHUBAuthor
Associate
April 11, 2025

@GMA wrote:

Hello @FZTHUB,

Using Main Speed Sensor in sensor less mode, and auxiliary Speed Sensor in encoder mode, motor does not spin?
If motor is able to spin, are the two electrical angle signals in phase?


Hello, thanks for your answer. Yes, that's correct – when I select the main speed sensor as sensorless and do not configure any auxiliary sensor, the motor runs.
However, as soon as I set the auxiliary sensor to encoder mode, the motor no longer starts.

So unfortunately, I’m not able to test whether the two electrical angle signals are in phase or not.

GMA
ST Technical Moderator
April 11, 2025

Hello @FZTHUB,

Does MC Motor pilot reports an error? 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA