Skip to main content
Visitor II
August 8, 2024
Question

Motor hold with 6-step algorithm

I'm building a motor for position control with a command rate ~10 Hz.  I'm using MCSDK 6.2.1 with a 6-step algorithm and Hall sensors.  The motor has a gear drive ratio ~400:1.  The output shaft has a rotary encoder for position.  I use the standard STM libraries for motor speed control and then manually implement position control based on encoder data.  

The problem is that the motor has to start/stop with almost every position command, and startup is unreliable.  On other projects using FOC I've found using a motor hold at 0 rpm helps - while the hold is not strong it makes the startup cleaner.  However the 6-step libraries do not support the hold at 0 rpm function.  Is there way to access this hold function in the 6-step libraries?  Or some other method for improved startup function?  Thanks in advance.

    This topic has been closed for replies.

    1 reply

    Roger SHIVELY
    ST Employee
    August 9, 2024

    Hello @CraigH

    This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

    Regards,

    Roger