Skip to main content
Zek_De
Senior
May 8, 2026 10:46 PM UTC
Question

Motor Driver Fully Isolated shunt reading

Hello everyone, I am currently working on a fully isolated motor driver using an STM32G474RE. I need to interface the AMC1301differential output to the MCU in a way that ensures accurate measurements. What is the best approach to achieve this? Also in mc workbench app, MCU opamp -> ADC hardware variant for Current sense -> InternalOpamps -> Differential -> InternalPGA. Or I will make the diff to single like in other picture wich looks easier. Also looks same with design below.

Zek_De_1-1778338412280.png

 



Zek_De_0-1778280329003.png

Zek_De_0-1778338366696.png

 

 

 

6 replies

MasterT
Lead II
May 10, 2026 8:56 PM UTC

G474re has ADC capable to run differential mode, so take example Fig.8-1. Power Vdd2 by 3.3V from st side to stay safe. I see amp has BW ~200 kHz, so if you are not designing low power kind of app., than run ADC at full scale, for 12- bits about 2.8 Msps and also set OVS - oversampling. Again, depends on required BW OVS may vary from 8- to max 256, and provide up to 16-bits resolution for free

 

Screenshot From 2026-05-10 16-46-27.png

Zek_De
Zek_DeAuthor
Senior
May 14, 2026 1:55 PM UTC

Zek_De_0-1778766665086.png

 

Zek_De_1-1778766689800.png

if I use amc1301 and diff mod of MCU , then what I will choose these numbers. for example 
Polarization offset -> 1.44? because 0 current mean amc1301 produce 1.44 V for each out, PGA = 0. what about offset network attenuation?. Or I will choose to convert to diff to single line and direct to MCU . I already know about that.  But diff mode advantage is two line can travel more in PCB without problem

MasterT
Lead II
May 14, 2026 3:31 PM UTC

My understanding, that those calculators were not designed for amc1301. So, select one option, use amc1301 and ditch calculators, or use calculators and ditch amc1301

Zek_De
Zek_DeAuthor
Senior
May 14, 2026 4:51 PM UTC

I think we can use it, 1.44 polarization, 1 is offset  network attenuation, but I want to be sure,because design is expensive no chance for mistake, I need an approve