Skip to main content
Associate III
Jun 12, 2025 8:57 AM UTC
Question

Motor current distorted at high speed

Hello,

I am using the FOC with hall sensor (having at 15 degree mechanical accuracy) on a BLDC motor controlled by STEVAL-PTOOL4A. I am using the MCSDK v6.3.2. 

I activated the Overmodulation in order to drive my motor at 18500RPM. However at this speed and without load I have a weird current signal. It is like a noise. However, when I run the motor at 8000RPM the signal is much better and it starts to be sinusoidal when I apply a load on my motor. 

Here are the current:
At  high speed no load

AnthonyK_0-1749718553237.png

At low speed no load:

AnthonyK_1-1749718596390.png

At low speed with load:

AnthonyK_2-1749718637963.png

 

Without OverModulation, at 17000 RPM with load:

AnthonyK_0-1749722001477.png

 

Can anyone help me with this.

Thank you.



 




This topic has been closed for replies.